We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
Overtorque detection level during power running
Function:
When the torque value is [F616: Overtorque detection level during power running] or more and remains over for the time specified by [F618: Overtorque detection time], tripping or alarm can be output. You can enable or disable the trip setting by [F615: Overtorque trip]. The trip display is "Ot".
You can output an alarm set regardless of the [F615] setting. Trip or alarm cannot be output when [F616] or [F617] is set to "0: Disabled".
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.