We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Related Information

Electronic thermal memory target

Function
Set a target to reset the integral value of overload at power off. It applies to both the motor electronic thermal and overload detection for inverter protection.
0: No.1 to 4 motor, memory disabled
2: No.1 motor, memory disabled
Reset the integral value. "0" applies to No.1 to 4 motors and "2" to the No.1 motor only.
1: No.1 to 4 motor, memory enabled
3: No.1 motor, memory enabled
For memory enabled, the overload integral values of the motor and inverter are saved at power off.
When power supply is ON again, the calculation process is resumed from the state when it is powered off.
However, with the RTC enabled (with operation panel), the subtraction process is performed according to virtual cooling curves, regardless of the setting.

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Need a Quote? Have A Question?
x









Processing...
Top Top