We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
Number of external equipment starting alarm
Function
This parameter counts the number of starting of the inverter, and when it reaches the value set by [F648: Number of starting alarm], it outputs the alarm and confirm it in [Monitor mode].
For number of external equipment starting alarm, you can outputs the alarm and confirm it in [Monitor mode]. For number of starting for external equipment, the number of input to the input terminal is counted.
Also, occurrence of the specified trip can be confirmed in [Monitor mode].
Signal output of the number of starting alarm of the inverter
This parameter counts the number of starting of the inverter, and when it reaches the value set by [F648: Number of starting alarm], it outputs the alarm and confirm it in [Monitor mode].
Output alarm
Assign "162: Number of starting alarm" to the unused output terminal.
[Monitor mode]
Set "100: Number of starting" to [F711: Monitor mode 1 display] through [F718: Monitor mode 8 display].
Signal output of the number of external equipment starting alarm
This parameter counts the number of starting of the external equipment, and when it reaches the values set by [F658: Number of external equipment starting alarm], it outputs the alarm and can be confirmed in [Monitor mode].
For Number of starting for external equipment, a signal to the input terminal with the function of "114: External equipment counter" is assigned is counted.
Output alarm
Assign "184: Number of external equipment starting alarm" to the unused output terminal.
[Monitor mode]
Set "103: External equipment counter" to [F711: Monitor mode 1 display] through [F718: Monitor mode 8 display].
Signal output of the number of occurrence of the specified trip
You can confirm occurrence of the specified trip in [Monitor mode]. You can set up to three specified trips.
Set the monitor numbers shown in the following table to [F711: Monitor mode 1 display] to [F718: Monitor mode 8 display].
"113: Number of specified trip 1"
"114: Number of specified trip 2"
"115: Number of specified trip 3"
Memo
The number of starting, the number of forward run, and the number of reverse starting up to the present time can be confirmed in [Monitor mode]. You can reset the monitor value to 0 with the setting of "12: Clear number of starting" in [tyP: Default setting].
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.