We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Related Information

Override multiplying input select

Function
You can make adjustment for adding or multiple to frequency command value by external signal.

Guideline for the setting
The override functions calculate the frequency command value by means of the following expression:
• Frequency command value × (1+[F661] Input (%)/100) + [F660] Input (Hz)
However, when the setting value of [F661: Override multiplying input select] is *1 in the table, use the following expression.
• Frequency command value × ([F661] Input (%)/100) + [F660] Input (Hz)

Additive override
An input override frequency is added to the frequency command value externally.
Example 1: [F660]= "3: Terminal II", [F661]= "0: Disabled"
Output frequency = Reference frequency + Override (terminal [II] input (Hz))
Example 2: [F660]= "1: Terminal RR", [F661]= "0: Disabled"
Output frequency = Reference frequency + Override (terminal [RR] input (Hz))

Multiple override
An input override frequency is added to the frequency command value externally.
Example 1: [F660]= "0: Disabled", [F661]= "3: Terminal II" [FMOd]= "1: Terminal RR", [FH]= "80.0", [UL]= "80.0"
terminal [RR] input
[F201]= "0", [F202]= "0.0", [F203]= "100", [F204]= "80.0"
terminal [II] input
[F216]= "0", [F220]= "0", [F218]= "100", [F221]= "100"
Output frequency = Reference frequency x {1 + Override (terminal [II] input (%)/100)}
Example 2: [F660]=0 (disabled), [F661]=1 (terminal [RR])
[FMOd]= "2: Terminal RX", [FH]= "80.0", [UL]= "80.0"
terminal [RX] input
[F210]= "0", [F211]= "0.0", [F212]= "100", [F213]= "80.0"
terminal [RR] input
[F201]= "0", [F205]= "0", [F203]= "100", [F206]= "100"
Output frequency = Reference frequency x {1 + Override (terminal [RR] input (%)/100)}
Example 3
Output frequency = Reference frequency x {1 + Override ([F729: Panel override multiplication gain] Setting value (%)/100)}

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Need a Quote? Have A Question?
x









Processing...
Top Top