We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
Terminal FP pulse train output function
Function
Pulse trains can be output from terminal [FP]. Set the pulse output function and the number of pulses.
Setting method
For example, to output frequency (0 - 60Hz) at 0 - 600 pulse, set as follows.
[FH]= "60.0", [F669]= "1", [F676]= "0", [F677]= "0.60"
When the item selected by [F676] has reached the value of the reference of maximum value, the number of pulse set by [F677: maximum pulse number of pulse train output] is output.
ON pulse width is a fixed width. When outputting the maximum number of pulses set by [F677], the width is fixed at a value, where the duty ratio is 50%.
Therefore, the duty ratio varies according to the output pulse.
For example,
• [F677]="0.80" (kpps), ON pulse width = approx. 0.6 (ms)
• [F677]="1.00" (kpps), ON pulse width = approx. 0.5 (ms)
• [F677]="1.60" (kpps), ON pulse width = approx. 0.3 (ms)
Pulses below 15pps cannot be output.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.