We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
Ot2: Overtorque 2
Cause:
1) The output current reached [F601: Stall prevention level 1] or more within the time set in [F452: Stall detection time during power running].
2) The power running torque reached [F441: Power running torque limit level 1] or more within the time set in [F452: Stall detection time during power running].
Clearing:
• Reduce the load.
• Lower the detection level of [F601] or [F441].
Discussion
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.