We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Related Information

Parameter mode select

Function
Select the display mode of parameter settings between [Setting mode] and [Easy mode].
You can select a mode at power on and use the operation key to switch it or see only [Easy mode].
How to read parameters depends on a mode.
[Easy mode]
• Register frequently set parameters as [Easy mode] parameters in advance. Only the registered parameters (up to 32) appear.
• Ten parameters are selected in the default setting. You can change them as required.
[Setting mode]
• You can read all parameters in the standard [Setting mode].
Selecting a setting value
0: Setting mode at power on
The parameter mode is set to [Setting mode] at power on. You can use the operation key to switch between [Setting mode] and [Easy mode].
• Operation panel: [ESC] key or [F1] key
• Extension panel: [EASY] key (if any)
1: Easy mode at power on
The parameter mode is set to [Easy mode] at power on.
You can use the operation key to switch between [Setting mode] and [Easy mode].
• Operation panel: [ESC] key or [F1] key
• Extension panel: [EASY] key (if any)
2: Easy mode only
The parameter mode is always [Easy mode].
You cannot see the [Setting mode] screen.
Setting parameters in [Easy mode]
Up to 32 parameters are displayed in [Easy mode]. Set among [F751: Easy setting 1] through [F782: Easy setting 32].
In [Easy mode], only parameters registered with [F751: Easy setting 1] through [F782: Easy setting 32] appear in the order of registration.
Set communication numbers of registered parameters for [F751: Easy setting 1] through [F782: Easy setting 32].

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Need a Quote? Have A Question?
x









Processing...
Top Top