We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Related Information

Default setting

Function
You can return parameters to their default settings at a time, clear run times, and store/rewrite parameters specified by users.
Note) The setting value becomes 0 after execution, but a check mark is added to the previous setting value.
Selecting a setting value
1: 50Hz setting
The following parameters are set for the base frequency 50 Hz.
Setting values of other parameters are not changed.
When you select a parameter and press the [OK] key, nothing appears momentarily, the same content displayed at power on appears, and the mode enters [Standard mode].
2: 60Hz setting
The following parameters are set for the base frequency 60Hz.
Setting values of other parameters are not changed.
When you select a parameter and press the [OK] key, nothing appears momentarily, the same content displayed at power on appears, and the mode enters [Standard mode].
3: Default setting 1
Return parameters except for some ones to their default settings.
When you select the setting and press the [OK] key, "Init" blinks in the main area and "Initializing" appears under it for a while.
They disappear momentarily, the same content displayed at power on appears, and the mode enters [Standard mode].
The history of past trip data is cleared.
To initialize all parameters, set [tyP: Default setting]to "13".
4: Clear past trips
Initialize (clear) the history information of eight past trips.
No parameter is changed.
When you select the setting and press the [OK] key, nothing appears momentarily, the same content displayed at power on appears, and the mode enters [Standard mode].
5: Clear cumulative run time
Clear cumulative run time to 0.
When you select the setting and press the [OK] key, nothing appears momentarily, the same content displayed at power on appears, and the mode enters [Standard mode].
6: Initialize typeform
Clear a trip if the type error "EtyP" occurs.
When you select the setting and press the [OK] key, nothing appears momentarily, the same content displayed at power on appears, and the mode enters [Standard mode].
7: Store user settings
Store the setting values of all current parameters.
8: Rewrite user settings
Rewrite the setting values of the parameters stored in "7: Store user settings" to the inverter.
You can use parameter initial settings specific for users with "7: Store user settings" and "8: Rewrite user settings."
9: Clear cumulative fan run time
Clear cumulative fan run time to 0.
Set it, for example, when you have replaced the cooling fan.
When you select the setting and press the [OK] key, nothing appears momentarily, the same content displayed at power on appears, and the mode enters [Standard mode].
12: Clear number of starting
Clear the values on the monitor to 0 for the number of starting, the number of forward starting, and the number of reverse starting.
When you select the setting and press the [OK] key, nothing appears momentarily, the same content displayed at power on appears, and the mode enters [Standard mode].
13: Default setting 2 (complete initialization)
Return all parameters to their default settings at a time.
When you select the setting and press the [OK] key, "Init" blinks in the main area and "Initializing" appears under it for a while.
They disappear momentarily, the same content displayed at power on appears, and the mode enters [Standard mode].
All parameters are returned to their default settings, and the history data of past trips is also cleared.

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Need a Quote? Have A Question?
x









Processing...
Top Top