We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Related Information

Etn1: Auto-tuning error 1

Cause:
1) The motor is not connected.
2) Something other than the motor is connected.
3) In the induction motor, an improper value, a synchronized motor speed value or a value close to it is set in [F417: Motor rated speed].

Clearing:
1) and 2) Check that the motor is connected.
3) Set [F417] according to the motor rating.
Discussion

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Need a Quote? Have A Question?
x









Processing...
Top Top