We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
Terminal RES function 2
Function
Default Settings
By default, the [F150 Terminal RES function 2] parameter will have the [0: No function] setting selected.
1.The [F153 Terminal RES function 2] is located under [5. Extended parameters]. Navigate to this option in the settings. Once the [5. Extended parameters] is highlighted select the [OK] button on this option.
2. Next highlight and select the [1 Input/Output parameters (F1--)].
3. Next scroll down using the trackpad of the remote until you highlight [F153 Terminal RES function 2]. Select this function by hitting the [OK] button on the remote.
4. All functions labeled with a "1" "2" or "3"all will be running at the same time when their corresponding switch is closed.
The adjustment range for the [F153 Terminal RES function 2] parameter ranges from 0-203.
Depending on which setting you have selected, that specific setting will force the inverter to perform the selcted setting. The inverter runs all the functions for that specified switch.
For example, when switch RES closes the inverter performs checks on all RES the functions. The [F153 Terminal RES function 2] parameter has the [0: No function] setting selected, the inverter also checks the function selected for [F113 Terminal RES function 1] and the inverter performs both functions, since all functions run when the RES switch is closed.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.
Register to view our materials and keep informed with our latest updates.
You may enter your filters below to locate manuals, brochures, software, drawings, and other important documents.
Select a category, choose a Product Family, then select from the list of available documents.
If you encounter any problems or have any questions please contact TIC-Webmaster@toshiba.com
Thanks for registering.
Please login with your email address.
Sign me up to receive future updates about Toshiba products
Yes No