Reverse inhibited

Function
This function limits the direction of rotation when the wrong Fwd or Rev run command is input.

F311 Adjustment Range:
0: Allowed
1: Rev inhibited
2: Fwd inhibited
3, 4: –
Important:
? When the motor is operated in the inhibited direction during operations such as preset speed operation with functions or jog run, the run command will be set to OFF.
? If the motor parameters are not set to the appropriate values when vector control or automatic torque boost is set, the motor may run in the reverse direction at approximately the slip frequency.
Set [F243: End frequency] to approximately the slip frequency.

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Scroll to Top