We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
Wakeup feedback
Function
This function is used to automatically decelerate and stop the inverter in the following case: the inverter continues to run at the frequency set with [LL: lower limit frequency], which has a low workload, for the period specified in [F256: Run sleep detection time] for energy saving, etc. (sleep function).
The LCD screen displays "LStP" during sleep.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.