We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Related Information

Short circuit detection at start

Function
Inverter detects inverter output short-circuit at the start.
Normally, short-circuit can be detected in the length of standard pulse (50 ?s). When operating a low-impedance motor, such as a high-speed motor, however, select the short-time pulse by [F614:Pulse width of short circuit detection at start] to prevent an error detection.

Setting the [F613: Short circuit detection at start]
0: At every startup by standard pulse
Detection is executed in the length of standard pulse every time at the start of inverter operation.
1: Only one time after power on by standard pulse
Detection is executed in the length of standard pulse only during the first start-up at power on or after resetting.
2: At every startup by F614 setting pulse
Detection is executed in the length of short-time pulse specified by [F614: Pulse width of short circuit detection at start] every time at the start of inverter operation.
3: Only one time after power on by F614 setting pulse
Detection is executed in the length of short-time pulse specified by [F614: Pulse width of short circuit detection at start] only one time during the first start-up at power on or after resetting.

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Need a Quote? Have A Question?
x









Processing...
Top Top