We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Related Information

Preset speed 30

The frequency commands can be switched with external logic signals.
For example, high speed and low speed are switched with 1-speed and 2-speed. Up to 31-speed can be set. They can be used as interruption frequency commands because they have priority over other frequency commands.
• They are valid in the case of run/stop with terminals. Set [CMOd: Run command select] to "0".
• Preset speed 16 to 31 are set only by terminal input. They cannot be set via communication.
• Preset speed 16 to 31 do not support preset speed with the functions. If these functions are required, select preset speed 1 to 15.

Reference of setting
Set the frequency to be used for preset speed 1 to 31 with [Sr1: Preset speed 1] to [F979: Preset speed 31].
When the preset speed command (external logic signal) is off, the frequency command set with [FMOd: Frequency command select 1] is valid.
When [FMOd: Frequency command select 1] is "12: Sr0", the setting value of [Sr0: Preset speed 0] becomes the frequency command.

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Need a Quote? Have A Question?
x









Processing...
Top Top